TLV320AIC3100 Audio Codec bringup - Clock issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TLV320AIC3100 Audio Codec bringup - Clock issue

3,888 次查看
divyeshmarne0
Contributor III

Hi Team, We are working on IXM8MM custom board. We are using tlv320aic3100 audio codec with imx8mm and Android 11 code base. Facing some issues related to MCLK. When I try to play audio, that time I can see 1.8V on MCLK, BCLK,WCLK lines (NO CLOCKS). if I change mclk to 49Mhz that time i can see clocks on I2S lines. In adb shell: evk_8mm:/sdcard # tinyplay LRMonoPhase4.wav Unable to open PCM device 0 (cannot set hw params: Invalid argument) LOGS: [ 939.481489] fsl-sai 30010000.sai: failed to derive required Tx rate: 1536000 [ 939.488611] fsl-sai 30010000.sai: ASoC: error at snd_soc_dai_hw_params on 30010000.sai: -22 Same query I have raised with TI. they are saying this codec only supports 12 and 12.5Mhz freq.. but when I am setting it to 12 and 12.5 , we are not getting clock output. TI suggested that please connect with vendor host for clock related issue. Attaching all the details from TI case.

0 项奖励
13 回复数

977 次查看
Adi99
Contributor I

Hii @divyeshmarne0

 

There are lots of questions and issues regarding tlv320aic31xx chip.

can you share your complete patch here ?

i have checked your 3100.patch file but its not working for me.

it would be great if you share more info.

i am facing sound-card issue error.

 

Thanks 

0 项奖励

3,469 次查看
Wobaffet
Senior Contributor I

Hello,

I hope you are doing well. We are planing to use the same codec for our project. Were you able to solve the problem? Thank you in advance.

Best Regards.

0 项奖励

3,464 次查看
divyeshmarne0
Contributor III
Yes.. We did all the changes, Now it is working

3,858 次查看
divyeshmarne0
Contributor III

Please find below update:

Measured all the clocks.

MCLK = 12.28 MHz
BCLK = 1.536  MHz
WCLK = 47.99 KHz

DIN = We can see data on DIN pin when we are playing audio file.

BUT SPEKER is not throwing any data . Not even noise. 

Please help to update the clock freq table .

Please check attached logcat logs and dmesg logs : 

4212.logcat.txt

 

.3426.dmesg.txt

all tinymix controls are off , Do you have any comment why DAC path is not enabled during boot time.

Latest changes:

--- a/sound/soc/codecs/tlv320aic31xx.c
+++ b/sound/soc/codecs/tlv320aic31xx.c
@@ -213,10 +213,12 @@ struct aic31xx_rate_divs {
/* 44.1k rate */
{12000000, 44100, 7, 5264, 128, 8, 2, 128, 8, 2},
{12000000, 44100, 8, 4672, 128, 6, 3, 128, 6, 3},
+ {12288000, 44100, 7, 5264, 128, 8, 2, 128, 8, 2},
{12500000, 44100, 7, 2253, 128, 8, 2, 128, 8, 2},
/* 48k rate */
{12000000, 48000, 8, 1920, 128, 8, 2, 128, 8, 2},
{12000000, 48000, 7, 6800, 96, 5, 4, 96, 5, 4},
+ {12288000, 48000, 8, 1920, 128, 8, 2, 128, 8, 2},
{12500000, 48000, 7, 8643, 128, 8, 2, 128, 8, 2},
/* 88.2k rate */
{12000000, 88200, 7, 5264, 64, 8, 2, 64, 8, 2},

Thanks

Divyesh.

0 项奖励

3,225 次查看
sabidi
Contributor I

Hi @divyeshmarne0  I have the same issue on clock can you please share your solution?

0 项奖励

3,220 次查看
divyeshmarne0
Contributor III

Hi Sabidi,

Are you using TLV320AIC3100 with imx8mm ?

0 项奖励

3,209 次查看
sabidi
Contributor I

I'm using Tlv320aic3254 with imx8mm

0 项奖励

3,204 次查看
divyeshmarne0
Contributor III

ok

0 项奖励

3,217 次查看
sabidi
Contributor I

I'm using tlv3245 with imx8mm

0 项奖励

3,212 次查看
divyeshmarne0
Contributor III

Hi Sab,

PFA patch.

0 项奖励

3,191 次查看
sabidi
Contributor I

Thank you for your quick replay, i'am using imx8mm with tlv320aic3254 on yocto, kernel version  5.4.127 and in my file drivers/clk/imx/clk-pll14xx.c b/drivers/clk/imx/clk-pll14xx.c i don't have static const struct imx_pll14xx_rate_table imx_pll1443x_tbl[], also in the codec tlv320aic3254 there isn't  struct aic31xx_rate_divs  struct aic31xx_rate_divs  struct aic31xx_rate_divs 

0 项奖励

3,870 次查看
divyeshmarne0
Contributor III

any update?

 

0 项奖励

2,586 次查看
Adi99
Contributor I
0 项奖励