We have two IMX6 processors in our system.One of the processor sends uncompressed video over UDP to other one. And there is also async. data communication (10 to 120 Bytes max) between each other using TCP . We experience sometimes dropped packets or sometimes transfer delay in the communication. We tried different methods in our source code. We also tried migrating the communication from TCP to UDP but we still see communication problems as before.
We did write some experimantal code for send/receive purposes between processors. We think sender side is able to send but the receiver side cannot receive all the packages sent.
We tried to suspend UDP video transfer while communication takes place and we saw that communication works flawlessly. But as sson as video transfer begins, the communication problem arises.
How can we debug the problem? Is there a possible solution we can try?
QT version : 5.3.2
UDP transfer : QUDPSocket
TCP transfer : ZMQ
Yocto : Poky Distro
Kernel : 3.14.28
Not only that, there should be heaps of statistics being kept by all of the driver layers to help you work out where things are going wrong.
It is possible that the "normal Linux tools" haven't been built into your distribution and you may need to enable some more of them in the build (usually in the Busybox configuration).
"ip link list" should list the links, and "ip -s link" should show you the link statistics, like it does on my desktop machine:
% ip -s link
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT group default qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
RX: bytes packets errors dropped overrun mcast
2484 27 0 0 0 0
TX: bytes packets errors dropped carrier collsns
2484 27 0 0 0 0
2: eno1: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc fq_codel master br0 state UP mode DEFAULT group default qlen 1000
link/ether 34:97:f6:8b:29:b5 brd ff:ff:ff:ff:ff:ff
RX: bytes packets errors dropped overrun mcast
436160163 690629 0 0 0 271599
TX: bytes packets errors dropped carrier collsns
18502209 111050 0 0 0 0
3: br0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue state UP mode DEFAULT group default qlen 1000
link/ether 34:97:f6:8b:29:b5 brd ff:ff:ff:ff:ff:ff
RX: bytes packets errors dropped overrun mcast
152022568 469297 0 0 0 0
TX: bytes packets errors dropped carrier collsns
36038066 74499 0 0 0 0
It is likely that the "ip" included with busybox doesn't give statistics. It doesn't on my old i.MX53 Linux. You'll have to see if your one does (or if your distribution comes with a "real one").
That means you have to dive into /proc/net and look at the snmp statistics:
# cat /proc/net/snmp
Ip: Forwarding DefaultTTL InReceives InHdrErrors InAddrErrors
ForwDatagrams InUnknownProtos InDiscards InDelivers OutRequests
OutDiscards OutNoRoutes ReasmTimeout ReasmReqds ReasmOKs
ReasmFails FragOKs FragFails FragCreates
Ip: 2 64 987 0 638 0 0 0 349 106 0 0 0 0 0 0 0 0 0
Icmp: InMsgs InErrors InDestUnreachs InTimeExcds
InParmProbs InSrcQuenchs InRedirects InEchos InEchoReps
InTimestamps InTimestampReps InAddrMasks InAddrMaskReps
OutMsgs OutErrors OutDestUnreachs OutTimeExcds OutParmProbs
OutSrcQuenchs OutRedirects OutEchos OutEchoReps
OutTimestamps OutTimestampReps OutAddrMasks OutAddrMaskReps
Icmp: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
Tcp: RtoAlgorithm RtoMin RtoMax MaxConn ActiveOpens
PassiveOpens AttemptFails EstabResets CurrEstab InSegs
OutSegs RetransSegs InErrs OutRsts
Tcp: 1 200 120000 -1 0 1 0 0 1 204 106 0 0 1
Udp: InDatagrams NoPorts InErrors OutDatagrams RcvbufErrors SndbufErrors
Udp: 0 0 0 0 0 0
UdpLite: InDatagrams NoPorts InErrors OutDatagrams RcvbufErrors SndbufErrors
UdpLite: 0 0 0 0 0 0
# cat /proc/net/snmp6
Ip6InReceives 17072
Ip6InHdrErrors 0
Ip6InTooBigErrors 0
Ip6InNoRoutes 0
Ip6InAddrErrors 0
Ip6InUnknownProtos 0
Ip6InTruncatedPkts 0
Ip6InDiscards 0
Ip6InDelivers 17072
Ip6OutForwDatagrams 0
Ip6OutRequests 36691
Ip6OutDiscards 0
Ip6OutNoRoutes 0
Ip6ReasmTimeout 0
Ip6ReasmReqds 0
Ip6ReasmOKs 0
Ip6ReasmFails 0
Ip6FragOKs 0
Ip6FragFails 0
Ip6FragCreates 0
Ip6InMcastPkts 4
Ip6OutMcastPkts 12
Ip6InOctets 6201232
Ip6OutOctets 3475704
Ip6InMcastOctets 448
Ip6OutMcastOctets 992
Ip6InBcastOctets 0
Ip6OutBcastOctets 0
Icmp6InMsgs 11
Icmp6InErrors 0
Icmp6OutMsgs 16
Icmp6OutErrors 0
... Lots more ...
Then you should look at the Ethernet statistics, which should be here:
# cd /sys/class/net/eth0/
# ls
addr_len carrier dormant flags iflink
operstate statistics type address dev_id
duplex ifalias link_mode power subsystem
uevent broadcast device features ifindex
mtu speed tx_queue_len
# cat duplex
full
# cat speed
100
# cd statistics
# ls
collisions rx_dropped rx_missed_errors
tx_carrier_errors tx_heartbeat_errors multicast
rx_errors rx_over_errors tx_compressed
tx_packets rx_bytes rx_fifo_errors
rx_packets tx_dropped tx_window_errors
rx_compressed rx_frame_errors tx_aborted_errors
tx_errors rx_crc_errors rx_length_errors
tx_bytes tx_fifo_errors
# cat *
0
0
9345077
0
0
0
0
0
0
0
0
0
26274
0
5570222
0
0
0
0
0
0
51206
0
The way to use these is to record all of the statistics after a clean power up, run your tests (that are dropping or running slow) and then record all the statistics after the test. Then see how many packets were sent from the sender, through TCP, out through Ethernet, then counted into the other one's Ethernet and up to TCP. You should be able to see the differences in packet counts, and see where packets are being dropped, and possibly why.
You should run TCP and you should make sure the flow-control works all the way through. Your sender shouldn't be able to push data faster than the receiver can read it. It is possible to get this programming wrong though (and have your software be the problem).
Let us know what you find.
Tom