Hello Team,
I want to know what all types of Camera sensors are supported in i.Mx6 Dual / Quad Series of SoC.
I am planning to use one of the listed camera sensors. Can you list which one will directly support/support with minimal changes?
Description | Part Number | Resolution |
Full camera + LED + ISP | V31105L Series | 1920x1080 |
Full camera + LED + ISP | MD-V22605L-74 | 1200x1080 |
Full camera + LED + ISP | B21105 Series | 1280x720 |
Sensor + ISP only | B164B03 SERIES | 1280x720 |
Sensor + ISP only | B31105 SERIES | 1920x1080 |
Sensor + ISP only | B36305 SERIES | 2592x1944 |
OV5640 | 2592x1944 | |
OH02A10 | 1920x1080 | |
OH08A40 | 4024x2180 |
Immediate help will be appreciated.
Thanks & Regards,
Kailas Kharse
current bsp supports ov5640 and ov5642 for imx6q as default
Hello Joanxie,
Our customer is insisting to use either of the camera listed, Can you please inform can we used this camera directly?
Video Format: MJPEG / YUV
Interface: USB 2.0 (Compliant with USB Video Class 1.1 Standard)
Frame Rate: 15~30 fps
Description | Part Number | Resolution | OD | Pixel Size | Interface | FPS | |
Full camera + LED + ISP | V31105L Series | 1920x1080 | 5.4 to 7.8 | 1.4 | USB | 15-30 | |
Full camera + LED + ISP | MD-V22605L-74 | 1200x1080 | 5.4 | 1.4 | USB | 30 | |
Full camera + LED + ISP | B21105 Series | 1280x720 | 5.5 | 1.4 | USB | 30 | |
Sensor + ISP only | B164B03 SERIES | 1280x720 | 3.24 | 1.12 | USB | 30-60 | |
Sensor + ISP only | B31105 SERIES | 1920x1080 | 4.9 | 1.4 | USB | 30 | |
Sensor + ISP only | B36305 SERIES | 2592x1944 | 5 | USB | 24 |
unfortunately these camera didn't be tested officially, if customer use usb camera, the bsp should support them as default, for performance, maybe you can check the link