Support of Broadcom radios on i.MX6Dual/DualPlus/Quad/QuadPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support of Broadcom radios on i.MX6Dual/DualPlus/Quad/QuadPlus

863 Views
mickaeltoumi
Contributor III

Hello,

Is it possible to confirm that the Broadcom based Murata solutions can be integrated on i.MXDual, DualPlus, Quad or QuadPlus.

I do see references to i.MX6UltraLite, SoloLite, SoloX, Solo and DualLite.

Thank you in advance for confirmation,

0 Kudos
Reply
2 Replies

730 Views
igorpadykov
NXP Employee
NXP Employee

Hi mickaeltoumi

yes it can be integrated too as mentioned on

http:/ /wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

730 Views
mickaeltoumi
Contributor III

Thanks igor, I have the confirmation I need.

0 Kudos
Reply