Hi
I'm currently streaming a USB Webcam from the IMX6Q SabreBoard to my computer over the network with this command:
gst-launch-0.10 v4l2src device=/dev/video0 ! 'video/x-raw-yuv,framerate=(fraction)30/1' ! ffmpegcolorspace ! vpuenc codec=12 ! multipartmux ! tcpserversink host=192.168.20.26 port=5000
This is working fine. When i use VLC, i can see the stream when typing the address tcp://192.168.20.43:5000
But i'd like to use the x264 codec. As i understood it, i just have to change the vpuenc codec=6 but this isn't working. I do receive a stream, but VLC tells me that the codec is undefined and that it can't decode it.
I'm pretty new with the use of streams so i'm kind of walking blindly. Is my gst-launch command correct for x264?
And moreover, how do i broadcast the stream instead of sending it directly to someone?
Best regards.
Ce message a été modifié par : Philippe Balleydier
已解决! 转到解答。
Pipeline for UDP-stream:
gst-launch udpsrc port=5000 caps=\"application/x-rtp, media=(string)video, clock-rate=(int)90000, payload=(int)96, encoding-name=(string)H264" ! rtph264depay ! ffdec_h264 ! xvimagesink
In attache ful script (server and client pipeline), tested on iMX53.
I managed to make it works thanks to kirill but i'm having issues with the Height and width of the stream
I use these 2 commands:
Server: gst-launch-0.10 v4l2src device=/dev/video0 ! 'video/x-raw-yuv,framerate=(fraction)30/1' ! ffmpegcolorspace ! vpuenc codec=6 ! rtph264pay ! udpsink host=192.168.20.26 port=5000
Client: gst-launch udpsrc port=5000 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, payload=(int)96, encoding-name=(string)H264" ! rtph264depay ! ffdec_h264 ! xvimagesink
The problem is, when i try to set the height and width of the stream, the pipeline won't create. I use this command for the server:
gst-launch-0.10 v4l2src device=/dev/video0 ! 'video/x-raw-yuv,height=720,width=1280,framerate=(fraction)30/1' ! ffmpegcolorspace ! vpuenc codec=6 ! rtph264pay ! udpsink host=192.168.20.26 port=5000$
(just added height=720,width=1280)
and the client console returns me:
ERROR: Pipeline doesn't want to pause.
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Could not negotiate format
Why can't i choose the height and width of the stream?
I tried like this:
gst-launch v4l2src capture-height=720 capture-width=1280 capture-mode=4 device=/dev/video0 ! 'video/x-raw-yuv,framerate=(fraction)30/1' ! ffmpegcolorspace ! vpuenc codec=6 ! rtph264pay ! udpsink host=192.168.20.26 port=5000
And it says:
WARNING: erroneous pipeline: no property "capture-height" in element "v4l2src0"
Those capture-height and width elements only exist on the module called mfw_v4lsrc but i'm using v4l2src.
v4l2src will have the property width and height, you can check that with gst-inspect v4l2src this command will display the properties of v4l2src
Try these commands
gst-launch v4l2src device=/dev/video0 ! video/x-raw-yuv,width=1280,height=720,format='(fourcc)'UYVY ! ffmpegcolorspace ! vpuenc codec=6 ! rtph264pay ! udpsink host=192.168.20.26 port=5000
gst-launch-0.10 -v v4l2src device=/dev/video0 ! 'video/x-raw-yuv,width=640,height=480' ! ffmpegcolorspace ! x264enc ! rtph264pay ! udpsink host=192.168.20.26 port=5000
I've tried multiple times the first line before. But i always get the same error:
ERROR: Pipeline doesn't want to pause.
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Could not negotiate format
For the second one, it's working, but i have big lag issues (at least a 10 seconds delay and not continuous at all)
I've observed this phenomenom multiple times with the x264enc module (i think it is not hardware optimized)
EDIT:
ok i've figured out the issue.
I usually use this command (a working one):
gst-launch v4l2src device=/dev/video0 ! 'video/x-raw-yuv,framerate=(fraction)30/1' ! ffmpegcolorspace ! vpuenc codec=6 ! rtph264pay ! udpsink host=192.168.20.30 port=5000
If i use the height and width parameters, they have to be quite low (like 320x240 or 640x480). If i try to set them too high (like 800x600, 1280x720), i have to reduce the framerate from 30 to 10, or i get the "Could not negotiate format" error.
Aren't we able to stream 720p30?
which USB camera are you using, have you check the driver settings for your camera whether it is having 720p resolution at 30fps
I tested it with ov5640 5mp camera in i.MX6q sabrelite board for that i have a 720p settings for 30fps and 15fps
Hello Philippe,
Try commands in the attached documents, these documents is specifically created for all the imx6 boards. In your case it is USB web cam for that you need to choose the appropriate video codecs. To find the available codecs give the command gst-inspect
Thanks
shan
Please try the following :
$ gst-launch-0.10 v4l2src device=/dev/video0 ! 'video/x-raw-yuv,framerate=(fraction)30/1' ! ffmpegcolorspace ! vpuenc codec=6 ! rtph264pay ! tcpserversink host=192.168.20.43 port=5000
For host VLC (sdp file) :
v=0
o=IN IP4 192.168.20.43
c=IN IP4 192.168.20.43
s=iMX6 GStreamer H264
m=video 5000 RTP/AVP 96
a=rtpmap:96 H264/90000
a=fmp:96 media=video; clock-rate=90000; encoding-name=H264
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your answer.
Do i copy/paste what you've written in a .SDP file and open it with VLC?
for the 'o' and 'c' parameters in de SDP file, Is it the IP of the receiving computer? (i've tried both anyway)
Because for now, it is not working. I do see a stream coming to the receiving computer on wireshark but it seems like VLC is unable to see it.
When i open the .SDP file with VLC and i go to "Statistics", the throughput received is 0Kb/s but codecs are recognized.
When i open a network stream with VLC (without using a .SDP file) with the address tcp://ip.of.sender:5000, i do get a throughput but nothing but a black screen (well, not a black screen, the VLC logo) (and plugin are not recognized)
Can the issue come from de Webcam?
I'm using a Microsoft Lifecam HD-3000 that worked well for mjpg streaming. Moreover, it is said that it is a UVC device. So i guess it should work properly.
Any ideas?
I'm missing the mfw_vpuencoder plugin. I found on the net that i need to add gst-fsl-plugin in the local.conf files and rebake. But the plugin is still missing? What packages do i need to include to make it work?