Greetings,
I need confirmation on a simple subject. If I connect the RESETBMCU of PF0100 to POR_B of i.MX6Q, when all the switching regulators are up and running at the PMIC, it will signal RESETBMCU for 2 to 4 ms. Only in this time interval, regarding the state of the BOOT_MODE[1:0] pins, processor will decided its one of three boot modes, internal boot, serial downloader and boot from fuses.
Thus by adding switches to BOOT_MODE pins, setting the pins to their designated values before the power up, as I give power to the PMIC, the boot mode will be set at the processor and there is no need to do anything else?
An example scenario is;
BOOT_MODE 1 is pulled to ground, BOOT_MODE 0 is pulled to 3V3, when pmic is powered up and all switching regulators are up, BOOT_MODE is set to 10 which corresponds to Internal Bootmode.
Did I understand this correct?
Regards,
Mete
已解决! 转到解答。
Hi Atilla
boot signals are latched some time after POR release, described in
sect.60.6.1.2.3 POR (SRC_POR_B) i.MX6DQ RM as:
"SRC will prepare the boot information and then de assert mmdc_rst_b."
after system_early_rst_b signal and PLLs locking and generation system root clocks.
Accurate time is not defined.
Recommended to have valid boot signals before POR release.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Atilla
boot signals are latched some time after POR release, described in
sect.60.6.1.2.3 POR (SRC_POR_B) i.MX6DQ RM as:
"SRC will prepare the boot information and then de assert mmdc_rst_b."
after system_early_rst_b signal and PLLs locking and generation system root clocks.
Accurate time is not defined.
Recommended to have valid boot signals before POR release.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------