Spread spectrum modulation of i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spread spectrum modulation of i.MX6UL

Jump to solution
2,175 Views
yuuki
Senior Contributor II

Dear all,

We want to enable the Spread spectrum modulation for DCLK of the LCD.

We observed a waveform by using spectrum analyzer.

LDB_DI0_CLK_SEL=PLL2 PFD3

CCM_CS2CDR: 0x020C402C = 0x0055B6EF

【SSCG-ON】Spread spectrum modulation enabled

CCM_ANALOG_PLL_SYSn: 0x020C8030 = 0x80002001

CCM_ANALOG_PLL_SYS_SS: 0x020C8040 = 0x05DC8006

CCM_ANALOG_PLL_SYS_DENOM: 0x020C8060 = 0x00000012

01_SSCG-ON.png

【SSCG-ON + DENOM setting】Spread spectrum modulation enabled + Denominator setting

CCM_ANALOG_PLL_SYSn: 0x020C8030 = 0x80002001

CCM_ANALOG_PLL_SYS_SS: 0x020C8040 = 0x05DC8006

CCM_ANALOG_PLL_SYS_DENOM: 0x020C8060 = 0x00001770

02_SSCG-ON+DENOMsetting.png

【SSCG-OFF】Spread spectrum modulation disabled

CCM_ANALOG_PLL_SYSn: 0x020C8030 = 0x80002001

CCM_ANALOG_PLL_SYS_SS: 0x020C8040 = 0x05DC0006

CCM_ANALOG_PLL_SYS_DENOM: 0x020C8060 = 0x00000012

03_SSCG-OFF.png

We suspect that setting is not enough

Is there a more necessary setting?

These setting is set by the imx6ul_clocks_init() function in the clk-imx6ul.c file of Yocto Linux BSP.

Should these registers be set in U-Boot too?

May I have advice?

Best Regards,

Yuuki

Labels (2)
0 Kudos
Reply
1 Solution
1,121 Views
art
NXP Employee
NXP Employee

Your Case #2 should work well producing the frequency deviation range of 6MHz and frequency modulation rate of 24kHz. Please note that you first have to set up the CCM_ANALOG_PLL_SYS_DENOM register and STOP and STEP fields of the CCM_ANALOG_PLL_SYS_SS register and only after that set the CCM_ANALOG_PLL_SYS_SS[ENABLE] bit. With other sequence, the spread spectrum function may not start properly.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,122 Views
art
NXP Employee
NXP Employee

Your Case #2 should work well producing the frequency deviation range of 6MHz and frequency modulation rate of 24kHz. Please note that you first have to set up the CCM_ANALOG_PLL_SYS_DENOM register and STOP and STEP fields of the CCM_ANALOG_PLL_SYS_SS register and only after that set the CCM_ANALOG_PLL_SYS_SS[ENABLE] bit. With other sequence, the spread spectrum function may not start properly.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,121 Views
yuuki
Senior Contributor II

Dear Artur-san,

Thank you for your support.

I'm sorry, we found it having got a wrong setting

We set PLL3 as a clock source for the LDB module.

I was able to confirm Spread spectrum by setting PLL2.

Best Regards,

Yuuki

0 Kudos
Reply