Sony image sensor connection to imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sony image sensor connection to imx6

2,368 次查看
erdani80
Contributor III

Hi,

 We are designing a board that will have two sony sensors and the image will be processed in an imx6.

 We are looking at solutions to convert from sub-lvds to parallel cmos interface.

 Has anybody a suggestion on a converter chip or solution we can use?, we are looking at a FPGA to do this but any comment is wellcomed.

Thanks,

  Daniel,

标签 (4)
标记 (3)
0 项奖励
回复
7 回复数

360 次查看
aneeshkumarvr
Contributor I

did you get any solution? thine has the chip sub-LVDS to parallel THC63LVD1024

0 项奖励
回复

356 次查看
erdani80
Contributor III

We used an FPGA and also implemented an ISP in the part.

1,773 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Daniel Amor,

There may be threads covering possible alternatives. FPGAs are certainly one, but it may be easier to use an available solution like the ADV7782.

http://www.analog.com/media/en/technical-documentation/data-sheets/ADV7782.pdf

I hope this helps!

Regards,

0 项奖励
回复

1,773 次查看
pks
Contributor I

Hello gusarambula,

I am curious whether you know if the ADV7782 not only supports the advertised OpenLDI LVDS, but also sub-LVDS which most Sony imaging sensors use. It seems like this might be the only alternative to using a Lattice FPGA solution.

0 项奖励
回复

1,773 次查看
erdani80
Contributor III

That could be an option, but we are targeting parallel camera sensor interface in the imx6 and this component uses serial MIPI.

I'll have a look at other analog parts, thanks :-)

0 项奖励
回复

1,734 次查看
jamiew
Contributor III

Hi @erdani80 

Did you ever find a device to do Sony LVDS to parallel MIPI on the i.MX6?

I need to do this as well.


Thanks

Jamie

0 项奖励
回复

1,729 次查看
erdani80
Contributor III

@jamiew , we placed an FPGA to do format conversion from sub LVDS to parallel video, and also some image processing to offload the processor