Some of the BT headset microphone does not work after reboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Some of the BT headset microphone does not work after reboot

跳至解决方案
1,049 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

 

      I am working on imx6q with Android Nougat. Some of the BT Headset microphone dose not work after reboot but speaker working fine.

      I checked with different BT headset and some of the headset I found this problem.

     

Please find the below log,

bt_bluegiga_headset: length:12 Data:SCO OPEN 255     

bt_bluegiga_headset: length:12 Data:SYNTAX ERROR

And also Please check the below working log,

bt_bluegiga_headset: length:10 Data:SCO OPEN 2
bt_bluegiga_headset: length:13 Data:CONNECT 4 SCO

Please response, If anyone in experience.

 

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar
标签 (4)
0 项奖励
回复
1 解答
929 次查看
vinothkumars
Senior Contributor IV

This one again verified in headset side, This is the problem with headset side. At first time it will work because we press volume button continuously for connecting purpose. But, after second time/once connected we are not pressing volume button, So, in this case it will not work.

I Closed this thread now.

Regards,

VInothS.

Regards,
Vinothkumar Sekar

在原帖中查看解决方案

0 项奖励
回复
2 回复数
930 次查看
vinothkumars
Senior Contributor IV

This one again verified in headset side, This is the problem with headset side. At first time it will work because we press volume button continuously for connecting purpose. But, after second time/once connected we are not pressing volume button, So, in this case it will not work.

I Closed this thread now.

Regards,

VInothS.

Regards,
Vinothkumar Sekar
0 项奖励
回复
929 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

This is the problem in custom bt headset side, Hands Free Profile Audio Gateway (HFP-AG) not working properly. This HFP-AG start once press the Volume button of the custom bt headset.

Please find the log, 

bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 READY
bt_bluegiga_headset: HFP-AG ID:3 Established 00:12:6f:04:f2:95
bt_bluegiga_headset: headset_uart_receive , rec_dataframe : HFP-AG 3 VOLUME 10, headsetBtStatus.hfpAg_linkId: 3
bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 VOLUME 10
bt_bluegiga_headset: headset_uart_receive , rec_dataframe : HFP-AG 3 UNKNOWN (0): AT+BTRH?\r, headsetBtStatus.hfpAg_linkId: 3
bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 UNKNOWN (0): AT+BTRH?\r
972 I bt_bluegiga_headset: headset_uart_receive , rec_dataframe : HFP-AG 3 UNKNOWN (0): AT+CSRSF=0,0,0,1,0,0,0\r, headsetBtStatus.hfpAg_linkId: 3
bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 UNKNOWN (0): AT+CSRSF=0,0,0,1,0,0,0\r

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar
0 项奖励
回复