Some of the BT headset microphone does not work after reboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some of the BT headset microphone does not work after reboot

Jump to solution
1,499 Views
vinothkumars
Senior Contributor IV

Dear NXP,

 

      I am working on imx6q with Android Nougat. Some of the BT Headset microphone dose not work after reboot but speaker working fine.

      I checked with different BT headset and some of the headset I found this problem.

     

Please find the below log,

bt_bluegiga_headset: length:12 Data:SCO OPEN 255     

bt_bluegiga_headset: length:12 Data:SYNTAX ERROR

And also Please check the below working log,

bt_bluegiga_headset: length:10 Data:SCO OPEN 2
bt_bluegiga_headset: length:13 Data:CONNECT 4 SCO

Please response, If anyone in experience.

 

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar
Labels (4)
0 Kudos
Reply
1 Solution
1,379 Views
vinothkumars
Senior Contributor IV

This one again verified in headset side, This is the problem with headset side. At first time it will work because we press volume button continuously for connecting purpose. But, after second time/once connected we are not pressing volume button, So, in this case it will not work.

I Closed this thread now.

Regards,

VInothS.

Regards,
Vinothkumar Sekar

View solution in original post

0 Kudos
Reply
2 Replies
1,380 Views
vinothkumars
Senior Contributor IV

This one again verified in headset side, This is the problem with headset side. At first time it will work because we press volume button continuously for connecting purpose. But, after second time/once connected we are not pressing volume button, So, in this case it will not work.

I Closed this thread now.

Regards,

VInothS.

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1,379 Views
vinothkumars
Senior Contributor IV

Dear NXP,

This is the problem in custom bt headset side, Hands Free Profile Audio Gateway (HFP-AG) not working properly. This HFP-AG start once press the Volume button of the custom bt headset.

Please find the log, 

bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 READY
bt_bluegiga_headset: HFP-AG ID:3 Established 00:12:6f:04:f2:95
bt_bluegiga_headset: headset_uart_receive , rec_dataframe : HFP-AG 3 VOLUME 10, headsetBtStatus.hfpAg_linkId: 3
bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 VOLUME 10
bt_bluegiga_headset: headset_uart_receive , rec_dataframe : HFP-AG 3 UNKNOWN (0): AT+BTRH?\r, headsetBtStatus.hfpAg_linkId: 3
bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 UNKNOWN (0): AT+BTRH?\r
972 I bt_bluegiga_headset: headset_uart_receive , rec_dataframe : HFP-AG 3 UNKNOWN (0): AT+CSRSF=0,0,0,1,0,0,0\r, headsetBtStatus.hfpAg_linkId: 3
bt_bluegiga_headset: process_headset_data Data:HFP-AG 3 UNKNOWN (0): AT+CSRSF=0,0,0,1,0,0,0\r

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar
0 Kudos
Reply