Hi,
Is there a way to determine the jitter specifications of the ENET1_REF_CLK for a RMII interface?
Thanks,
Scott
For the RMII interface, the reference clock should be 50MHz +/- 50ppm.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
We are using a 24 MHz +/- 30 ppm crystal for the SoloX XTAL. Similar to what is used on the SoloX Sabre board. But that is the frequency tolerance, we are looking for a way to figure out if there is a jitter specification for what the SoloX is able to output for the 50 MHz RMII clock to the PHY.