SoC's I/I vs Processing Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SoC's I/I vs Processing Speed

485 Views
barnabasmogan
Contributor I

I am looking for a 1.6 GHz or faster SoC with at least 6 UARTs (among other features). I found one with 6 UARTs but it runs at 1 GHz:

i.MX 6Solo (Cortex A9, Cortex M4) with 6 UARTs, but this runs at 1 GHz: http://cache.freescale.com/files/32bit/doc/brochure/FLYRIMXPRDCMPR.pdf

I am finding that it is common to use a LPC (Low Pin Count) bus and add on I/O / Super I/O / Controller Hubs to add additional I/O support.

I would like to minimize development with these features integrated into the chip. There are a few others out there that come close but I still haven't found what I am looking for.

Does anyone have any recommendations ? Thank you.

Labels (1)
Tags (2)
0 Kudos
1 Reply

446 Views
igorpadykov
NXP Employee
NXP Employee

Hi Barnabas

for such high speed processors one can look at

QorIQ Processors Based on ARM Technology

QorIQ LS2080A and LS2040A|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos