[iMX6Q] No SDCLK for DDR3.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[iMX6Q] No SDCLK for DDR3.

Jump to solution
812 Views
chilwonna
Contributor II

Hi,

I made a new board from SABRESDP_C5.

DDR3's configuration is  same with SABRESDP_C5.

But, I have a big problem about DDR3.

In DDR Stress Test Tool,

Address and Data lines is generated. But SDCLK is not.

I need a help. Please advise.

Labels (1)
Tags (3)
0 Kudos
1 Solution
685 Views
igorpadykov
NXP Employee
NXP Employee

Hi chillwona

probably these traces are shorted or broken, may be recommended

to check layout. Also please check Chapter 8 Avoiding Board Bring-up Problems

i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
685 Views
chilwonna
Contributor II

thanks.

solved.

0 Kudos
686 Views
igorpadykov
NXP Employee
NXP Employee

Hi chillwona

probably these traces are shorted or broken, may be recommended

to check layout. Also please check Chapter 8 Avoiding Board Bring-up Problems

i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos