All,
I am having difficulty communicating with my iMX6Q. I am ssh'ed in and symbols appear after some delay. Pinging from the iMX6 to my router, reveals a delay of 100ms! My computer to the iMX6 is 500ms!
Could anyone offer any debugging advice? Thank you in advance!
Constantin
已解决! 转到解答。
Please try the solution, suggested in
https://community.freescale.com/message/319417#319417
(adding "enable_wait_mode=off" in the bootargs of U-boot)
Hey Leonardo, I am using the L.3.0.35_1.1.0_121218 uboot binary (u-boot-mx6q-sd.bin) and oneiric file system. I believe I got these from the Downloads sections but I'm having trouble finding them again.
What am I looking for with the ssh -v flag? It seems the entire connection is slow (due to the ping tests?) Thank you
It may be a DNS issue on your side: http://scofaq.aplawrence.com/FAQ_scotec4slow_ping.html
Also, try another filesystem, like the Linux Demo Image; if problem persists, then something is wrong on your network.
Hey Leonardo, thanks for the link! I tried the ping -n, but experienced the same ping. We have a few other systems running on the network (currently turned off), they do not experience the similar latency's.
My first thought is that this is something I've done in setting up the board (perhaps in uboot?) and is related to a driver setting or maybe version?