Slow Network on SABRE iMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Slow Network on SABRE iMX6Q

Jump to solution
2,033 Views
constantins
Contributor II

All,

I am having difficulty communicating with my iMX6Q. I am ssh'ed in and symbols appear after some delay. Pinging from the iMX6 to my router, reveals a delay of 100ms! My computer to the iMX6 is 500ms!

  Could anyone offer any debugging advice? Thank you in advance!

Constantin

Labels (2)
0 Kudos
Reply
1 Solution
1,627 Views
Yuri
NXP Employee
NXP Employee

Please try the solution, suggested in


https://community.freescale.com/message/319417#319417

(adding "enable_wait_mode=off" in the bootargs of U-boot)

View solution in original post

0 Kudos
Reply
7 Replies
1,628 Views
Yuri
NXP Employee
NXP Employee

Please try the solution, suggested in


https://community.freescale.com/message/319417#319417

(adding "enable_wait_mode=off" in the bootargs of U-boot)

0 Kudos
Reply
1,627 Views
constantins
Contributor II

Yuri thank you very much, the difference was instantly visible. Tried booting again without the suggested parameter and the problem re-emerged.

0 Kudos
Reply
1,627 Views
LeonardoSandova
Specialist I

Which BSP version are you using ? L3.0.35_1.1.0? Also, for a more verbose log, add -v to the ssh command

Leo

0 Kudos
Reply
1,627 Views
constantins
Contributor II

Hey Leonardo, I am using the L.3.0.35_1.1.0_121218 uboot binary (u-boot-mx6q-sd.bin) and oneiric file system. I believe I got these from the Downloads sections but I'm having trouble finding them again.

What am I looking for with the ssh -v flag? It seems the entire connection is slow (due to the ping tests?) Thank you

0 Kudos
Reply
1,627 Views
LeonardoSandova
Specialist I

It may be a DNS issue on your side: http://scofaq.aplawrence.com/FAQ_scotec4slow_ping.html

Also, try another filesystem, like the Linux Demo Image; if problem persists, then something is wrong on your network.

0 Kudos
Reply
1,627 Views
constantins
Contributor II

Hey Leonardo, thanks for the link! I tried the ping -n, but experienced the same ping. We have a few other systems running on the network (currently turned off), they do not experience the similar latency's.

My first thought is that this is something I've done in setting up the board (perhaps in uboot?) and is related to a driver setting or maybe version?

0 Kudos
Reply
1,627 Views
LeonardoSandova
Specialist I

I do not think it is U-boot related problem. U-boot is just the loader and you are having issues on the OS.

0 Kudos
Reply