I was wondering if it is possible to have SPIBlockingTransfer, SPINonBlockingTransfer (Interrupt Based) and SPISdmaTransfer all 3 working at the same time? I am using an i.MX8. Would I continuously have to Enable and Disable SPI SDMA constantly to achieve this? I would like to have some operations to happen over DMA while others to happen directly. I am not sure if this is even possible. Has anyone tried this?
I am trying to get this to work on an IMX8MQ on the Cortex M4 side. I have an EVK-MIMX8MQ board and trying to get this to work on that. I downloaded the SDK from the NXP website for the eval board.