Everyone,
I was wondering if anyone has tried to carry out signed updates according to the instructions in section 5.2 of the R13.4 Advanced User Guide? Although unsigned updates seem to work fine, I get the following error message when trying to call sign_target_files_apks
File "./build/tools/releasetools/sign_target_files_apks", line 349, in <module> main(sys.argv[1:])
File "./build/tools/releasetools/sign_target_files_apks", line 328, in main misc_info = common.LoadInfoDict(input_zip)
File "/home/.../.../build/tools/releasetools/common.py", line 111, in LoadInfoDict
raise ValueError("can't find recovery API version in input target-files")
ValueError: can't find recovery API version in input target-files
I am passing the ota zip from the make ... dist target. I am wondering if this is similar to the problem discussed at: Google Groups
I have gone through the process to generate the keys and made sure the directory referencing those keys are passed to the sign_target_files_apks call.
Michael Robbeloth
Hello, Michael:
I made one experiment by following the suggestions of guideline and it can work. For example:
1. Created and switch to the folder vendor/fsl/security/sabresd_6dq/
2. Created keys and key in the passwords:
3. In android root folder, run the command and key in passwords:
~/android/build/tools/releasetools/sign_target_files_apks -d vendor/fsl/security/sabresd_6dq/ out/dist/sabresd_6dq-target_files.zip signed-target_files.zip
4. The command can run well.
Xiaoli,
This is the procedure I followed and it matches up with section 5.2 of the R13.4 Advanced User Guide. However, this does not correct the particular problem I am facing. If it makes a difference, my organization is using Ubuntu 10.04 LTS release on this system.
Michael Robbeloth