Shutdown issue with imx6 sabre-sd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shutdown issue with imx6 sabre-sd

402 Views
divyeshpatel
Contributor I

Hi, 

        Currently, I am working on imx6 sabre-sd board. I am facing issue with shutdown. I ported Marshmallow OS on my custom board. When I am doing "reboot -p " command. It is going for halted. and after some interval, device is restarted automatically. 

       Can anyone give me suggestion related this issue ??

Thanks, 

Divyesh

0 Kudos
1 Reply

349 Views
igorpadykov
NXP Employee
NXP Employee

Hi Divyesh

reason may be that i.MX6Q Sabre SD board starts automatically when applied power,

to prevent it one can try to implement additional "OPTIONAL: PMIC Power On Circuit"

described on spf-27392 p.19 Sabre board schematic

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
SABRE Platform for Smart Devices|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos