Sharing boot_cfg lines

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sharing boot_cfg lines

ソリューションへジャンプ
809件の閲覧回数
jautry
Contributor IV

I noted on the eval board that Boot-Cfg input lines to the processor MIMXRT 1062  were shared.  Is it possible to share these lines since they are only accessed at startup for config data?  Is the way to do this is to start with them configured for Boot-Cfg and after boot changing the line configuration?

0 件の賞賛
1 解決策
791件の閲覧回数
Yuri
NXP Employee
NXP Employee

@jautry 
Hello,

  The default pins state are configured after boot configuration is latched.

Regards,
Yuri

 

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
803件の閲覧回数
Yuri
NXP Employee
NXP Employee

@jautry 
Hello,

  Section 9.4.2 (GPIO boot overrides) of the RM contains information about the boot override pins.

https://www.nxp.com/webapp/Download?colCode=IMXRT1060RM

  After boot these pins can be used for other functionality.
Use i.MX Pins tool for possible configurations.

https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX

Regards,
Yuri.

0 件の賞賛
797件の閲覧回数
jautry
Contributor IV

I just want to make sure.  The config tool lists the GPIO as the default at power up but not the config option.  So the default is actually the config option for reading the boot configs and then the mux is executed to direct the pins to proper configuration.  We do not have to specifically define the pin for config option.

0 件の賞賛
792件の閲覧回数
Yuri
NXP Employee
NXP Employee

@jautry 
Hello,

  The default pins state are configured after boot configuration is latched.

Regards,
Yuri

 

0 件の賞賛