I want to set up the WiFi and Bluetooth(WL1835) on our custom board, where also it is connected to SD2 interface(WiFi) and UART2(BT). Now my question is I have drivers in the kernel 3.14.28 for wlcore, wl18xx and bluetooth ,will this driver code will work or I need to modify something?
If I need to modify then what part of the driver I need to modify?
Do I need to make changes in Device tree ?
Can I access the WiFi at u-Boot level, if yes then How?
one can follow 3.10.53 bring-up steps
Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53
Best regards
igor
Hello,
TI has the wiki page for integration with i.MX
http://processors.wiki.ti.com/index.php/WL18xx_First_Time_Getting_Started_Guide_(IMX6)
Luis