Hi,
I am working on an audio application using an i.MX6ULL and I need to use the hardware ASRC of the processor with the S/PDIF RX clock on the asrc pair input.
The problem I have I that even after the S/PDIF dpll is locked I can't read the rate of the spdif_rx_clk so the pair configuration fails to calculate the input divisor.
In the reference manual I read that after the spdif dpll is locked the received rate is directly generated to spdif_rx_clk. Is that right or are there registers to configure to make it go through to the asrc controller?
Thank you,
Manuel BA
解決済! 解決策の投稿を見る。
Hi Manuel
S/PDIF RX clock is described in sect.50.4.1.8
i.MX 6ULL Applications Processor Reference Manual
some spdif tests which may be useful:
doc\mxc_spdif_test\test - imx-test - i.MX Driver Test Application Software
doc\mxc_asrc_test\test - imx-test - i.MX Driver Test Application Software
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Manuel
S/PDIF RX clock is described in sect.50.4.1.8
i.MX 6ULL Applications Processor Reference Manual
some spdif tests which may be useful:
doc\mxc_spdif_test\test - imx-test - i.MX Driver Test Application Software
doc\mxc_asrc_test\test - imx-test - i.MX Driver Test Application Software
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thank you for your answer, I have been able to recover the RX clock in the asrc module.
I also have opened another question about the asrc clock sources.
Manuel