Dear all
I want to set gpio for pinctrl_enet_irq such as
pinctrl_enet_irq: enetirqgrp {
fsl,pins = <
MX6QDL_PAD_SD1_DAT1__GPIO1_IO17 0x000b1
>;
};
but the irq always -1, is anysome wrong ?
Thanks
Hi bordon
according to ERR006687 only GPIO6 can be used:
All of the interrupts can be selected by MUX and output to pad GPIO6.
http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------