Set MX6QDL_PAD_SD1_DAT1__GPIO1_IO17 for pinctrl_enet_irq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set MX6QDL_PAD_SD1_DAT1__GPIO1_IO17 for pinctrl_enet_irq

525 Views
bordonkuo
Contributor II

Dear all
    
I want to set gpio for pinctrl_enet_irq such as
 
        pinctrl_enet_irq: enetirqgrp {
            fsl,pins = <
                MX6QDL_PAD_SD1_DAT1__GPIO1_IO17        0x000b1
            >;
        };
 
but the irq always -1, is anysome wrong ?
 
 
 
 
 
Thanks

Labels (1)
0 Kudos
1 Reply

410 Views
igorpadykov
NXP Employee
NXP Employee

Hi bordon

according to ERR006687 only GPIO6 can be used:
All of the interrupts can be selected by MUX and output to pad GPIO6.
http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos