Segmentation fault in Linux 3.10.17

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Segmentation fault in Linux 3.10.17

484件の閲覧回数
alexlevandovski
Contributor I

Hello.

I use Linux 3.10.17 kernel, imx6qsabresd. If I try to run /opt/viv_samples/vdk/.... Vivante examples - I get the Error: Segmentation fault.

Also, if I try to start   X.Org X Server 1.14.4, I get the same Error. Who knows this Problem? Do you have solutions?

Thanks for any help in adwance.

Alex

ラベル(1)
0 件の賞賛
1 返信

404件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alex

one can try to build images from

linux-2.6-imx.git - Freescale i.MX Linux Tree 

However since this release is not present on official product page

i.MX 6 Series Software and Development Tool|NXP 

this means that it is not more supported and recommended to use more new

releases.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛