Hi,
I am able to build the u-boot with secure boot feature enabled. But the below command not showing any HAB Block details..
The below is my command for that.
./tools/mkimage -n board/freescale/mx6sabresd/mx6dl_fs053_nt5cc256m16ep-ek-RA_Ver.cfg.cfgtmp -T imximage -e 0x17800000 -d u-boot-dtb.bin u-boot-dtb.imx
and this command shows output like below.
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 663552 Bytes = 648.00 KiB = 0.63 MiB
Load Address: 177ff420
Entry Point: 17800000.
What is missing for my u-boot?
Why its not showing HAB Blocks?
Used uboot version : 2018.03
Thanks