SabreSD board - SD card preparation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SabreSD board - SD card preparation

1,193件の閲覧回数
supriyac
Contributor I


Hello Team,

Am trying to boot sabresd board with the my compiled images. (uboot and kernel)

Could you please provide me with sd card preparation procedure?

Also am trying to get rootfs.tar via buildroot

Am facing two problems when following below link:

(Buildroot for the i.MX6 sabre sd platform in a few commands )

1. getting error during configuration as

make[1]: *** No rule to make target `freescale_imx6sabresd_defconfig'.  Stop.

2. Kernel not booting

mmc1 is current device

** Unrecognized filesystem type **

** Unrecognized filesystem type **

Booting from net ...

FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !

0 件の賞賛
返信
2 返答(返信)

679件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to section 4.3 (Preparing an SD/MMC card to boot) of the "i.MX_Linux_User's_Guide.pdf"

of the recent NXP BSP (please use it) :

https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_MX6QDLSOLO&appType=license&location=null&...

Summary page :

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

679件の閲覧回数
supriyac
Contributor I

Thank you Yuri.

0 件の賞賛
返信