Sabre Board_Ethernet PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabre Board_Ethernet PHY

787件の閲覧回数
hareeshth
Contributor I

Hi,

Is there any equivalent part for QUALCOMM ATHEROS AR8031-AL1B Module.

Regards,

Hareesh

ラベル(1)
0 件の賞賛
1 返信

457件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hareesh

AR8033 is a less expensive version of the AR8031 as it does not have the 1588 support.

However on web there has been some information that direct replacement leads

to link speed issues, so seems some modification of drivers needed.

Also other phy can be used, such as KSZ9021

http://boundarydevices.com/product/sabre-lite-imx6-sbc/?gclid=CKvP5PTSisgCFYQRHwodqdIOVw

broadcom phy

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛