SW workaround for i.MX8MQ e11231 for newer BSPs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SW workaround for i.MX8MQ e11231 for newer BSPs

411 次查看
RayW8d
Contributor I

Hi,

I have received the patches of SW workaround for i.MX8MQ e11231 in a previous thread Re: SW workaround for i.MX8MQ e11231: USB: Clock m... - NXP Community from @igorpadykov. However, I have found the patches are from the year 2019 and can only be directly applied to old source trees.

I have adapted the old patches to the newer BSPs that are using linux-imx of imx_5.4.70_2.3.0/lf-5.10.y branches and imx-atf of imx_5.4.70_2.3.0/lf_v2.4 branches but have no success so far since it turns out that the system cannot be waked up by any USB devices.

I'd like to ask if there are any new patches for newer BSPs or any advice that could help me adjust the old patches for newer BSPs?

Thanks in advance.

BR
Ray

0 项奖励
回复
1 回复

402 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ray

 

there are no plans for implementing these patches in bsps, in general help

for porting patches is provided using  https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 项奖励
回复