I want to access the board from network so How to enable SSH on I.Mx8mmini.
You need to have ssh server installed and running on i.MX board to be able to access the board from PC .
So you need to install some ssh server (for example openssh-server).
And then you need to make sure that is is turned on as service with the command like "/etc/init.d/ssh status".
And of course you need to make sure that network configuration (hardware and routing) connects the PC and i.MX board.
Thanks for replying, i Want to know how to configure in yocto as i got the below error message
ERROR: fsl-image-validation-imx-1.0-r0 do_rootfs: Could not invoke dnf. Command '/home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/recipe-sysroot-native/usr/bin/dnf -y -c /home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/rootfs/etc/dnf/dnf.conf --setopt=reposdir=/home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/rootfs/etc/yum.repos.d --repofrompath=oe-repo,/home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/oe-rootfs-repo --installroot=/home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/rootfs --setopt=logdir=/home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/temp --nogpgcheck install gst-plugins-good packagegroup-core-boot gst-plugins-bad apt weston-init gst-plugins-base-ffmpegcolorspace gst-plugins-good-udp packagegroup-tools-bluetooth run-postinsts tzdata gstreamer1.0-rtsp-server mariadb dhcpcd python3-pip gst-plugins-good-rtsp gst-plugins-base-videotestsrc home-assistant psplash xterm python apache2 python3-opencv gstreamer1.0 python-flask gst-openmax weston-xwayland libcgroup python3 gst-plugins-good-rtpmanager gstreamer1.0-plugins-good dhcp-server init-ifupdown python-core openssh gst-plugins-good-matroska packagegroup-fsl-gstreamer1.0-full packagegroup-fsl-tools-benchmark gst-fluendo-mpegdemux gst-plugins-good-rtp python-pip packagegroup-core-tools-debug gst-variable-rtsp-server packagegroup-core-ssh-dropbear v4l-utils gstreamer1.0-plugins-ugly-meta gtk-doc gst-plugins-ugly packagegroup-fsl-tools-gpu packagegroup-core-tools-testapps packagegroup-core-tools-profile gstreamer1.0-plugins-bad packagegroup-base-extended gsoap connman-client packagegroup-fsl-tools-audio packagegroup-core-nfs-server libnss-mdns packagegroup-fsl-tools-gpu-external gstreamer1.0-plugins-ugly packagegroup-fsl-gstreamer1.0-commercial ntp imx-gst1.0-plugin apache-websocket packagegroup-core-full-cmdline packagegroup-fsl-gstreamer1.0 packagegroup-fsl-tools-testapps gst-plugins-base-ogg dhcp-client gstreamer1.0-plugins-base php connman locale-base-en-us locale-base-en-gb' returned 1:
Added oe-repo repo from /home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/oe-rootfs-repo
Last metadata expiration check: 0:00:01 ago on Thu 14 Nov 2019 02:21:16 PM UTC.
Error:
Problem: package packagegroup-core-ssh-dropbear-1.0-r1.noarch requires dropbear, but none of the providers can be installed
- package openssh-7.6p1-r0.aarch64 conflicts with dropbear provided by dropbear-2017.75-r0.aarch64
- conflicting requests
(try to add '--allowerasing' to command line to replace conflicting packages or '--skip-broken' to skip uninstallable packages)
ERROR: fsl-image-validation-imx-1.0-r0 do_rootfs: Function failed: do_rootfs
ERROR: Logfile of failure stored in: /home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/tmp/work/imx8mmevk-poky-linux/fsl-image-validation-imx/1.0-r0/temp/log.do_rootfs.32231
ERROR: Task (/home/santhosh/Desktop/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb:do_rootfs) failed with exit code '1
How to resolve this error
Regards
Santhosh kumar
Hi santhoshkumar
I use the image imx-boot-imx8mmevk-sd.bin-flah_evk but it doesn't integrate openssh, do you know how to add it?
And how do you check that it is activated?
There has to be a ssh.service right?
Regards
Iñigo