SPL to u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,558件の閲覧回数
Arm7
Contributor II

Hello, 

Is there a way to pass info from SPL to u-boot ?

In SPL I read a fuse and I have to pass it to u-boot.

Thank you!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,486件の閲覧回数
dtony
Contributor III

 

 

Maybe you can try HANDOFF

config HANDOFF
bool "Pass hand-off information from SPL to U-Boot proper"
depends on BLOBLIST
help
It is useful to be able to pass information from SPL to U-Boot
proper to preserve state that is known in SPL and is needed in U-Boot.
Enable this to locate the handoff information in U-Boot proper, early
in boot. It is available in gd->handoff. The state state is set up
in SPL (or TPL if that is being used).

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,487件の閲覧回数
dtony
Contributor III

 

 

Maybe you can try HANDOFF

config HANDOFF
bool "Pass hand-off information from SPL to U-Boot proper"
depends on BLOBLIST
help
It is useful to be able to pass information from SPL to U-Boot
proper to preserve state that is known in SPL and is needed in U-Boot.
Enable this to locate the handoff information in U-Boot proper, early
in boot. It is available in gd->handoff. The state state is set up
in SPL (or TPL if that is being used).

0 件の賞賛
返信
4,500件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Arm7 

The uboot will query storage first, if there is no env, it will directly use the env at compile time.

Best regards

Harvey

0 件の賞賛
返信