Has anyone ever tried to run a SPI device off the Audio Code Header on the iMX 25 PDK Personality board? I have a chip with an SPI interface, but it has a few quirks. I need to experiment with the chip first to decide if "so broke" we have to bit-bang it or if the SPI interface on the chip is functional enough to run over SPI. That seems like the easiest access point to an SPI port, but curious if anyone else has tried it. Or if there is a better solution I'm not seeing ....
Hi
i'm working with nucleus ready start on the spi ,actualy i'am trying to make something work with the lwspi driver ,but the problem is that i don't really know how to start ,and the nucleus approach is new to me .