SOM/SOC to access 32-bit data from external static memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SOM/SOC to access 32-bit data from external static memory

ソリューションへジャンプ
508件の閲覧回数
htran
Contributor I

Hi All,

I am looking for a System-on-Module / System-on-chip that has  32-bit static memory interface (or 32-bit parallel bus) in order to  read 32-bit data from external FIFO (SN74V3690). I used LH79524 before and wonder if there is a similar one?

I have been looking at iMX6 and iMX7 but most of them only has 16-bit static memory interface.

I'm really new into this area so please kindly advise.

Thank you,

タグ(2)
0 件の賞賛
1 解決策
466件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  i.MX6 EIM supports 8 / 16 / 32 Bit data port for Non Multiplexed Address / Data Mode, and

16 / 32 Bit Multiplexed Address / Data mode. Use "EIM multiplexing" table in i.MX6 RM(s).

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

0 件の賞賛
1 返信
467件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  i.MX6 EIM supports 8 / 16 / 32 Bit data port for Non Multiplexed Address / Data Mode, and

16 / 32 Bit Multiplexed Address / Data mode. Use "EIM multiplexing" table in i.MX6 RM(s).

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛