Getting VSC8502 working with iMX8QM (device tree and driver patch).
dts file changes:
#include <dt-bindings/net/mscc-phy-vsc8531.h>
...
&fec2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec2>;
clocks = <&enet1_lpcg 4>,
<&enet1_lpcg 2>,
<&enet1_lpcg 0>,
<&enet1_lpcg 1>;
phy-mode = "rgmii-rxid"; // Phy drives Rx clock. Tell Phy driver, mscc_main.c to delay clock 2 nS
phy-handle = <ðphy0>;
fsl,magic-packet;
nvmem-cells = <&fec_mac1>;
nvmem-cell-names = "mac-address";
fsl,rgmii_txc_dly; // i.MX8 drives Tx clock. Delay Tx clock
status = "okay";
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-id0007.0630","ethernet-phy-ieee802.3-c22";
vsc8502,vddmac = <2500>;
vsc8502,edge-slowdown = <10>; // recommended for VDDMAC=2500 mV
vsc8502,led-0-mode = <VSC8531_LINK_ACTIVITY>;
vsc8502,led-1-mode = <VSC8531_LINK_10_100_ACTIVITY>;
vsc8502,led-2-mode = <VSC8531_LINK_1000_ACTIVITY>;
};
};
};
...
pinctrl_fec2: fec2grp {
fsl,pins = <
IMX8QM_COMP_CTL_GPIO_1V8_3V3_ENET_ENETA_PAD 0x000014a0
IMX8QM_ENET1_REFCLK_125M_25M_CONN_ENET1_REFCLK_125M_25M 0x06000020
IMX8QM_ENET1_MDC_CONN_ENET1_MDC 0x06000020
IMX8QM_ENET1_MDIO_CONN_ENET1_MDIO 0x06000020
IMX8QM_ENET1_RGMII_TX_CTL_CONN_ENET1_RGMII_TX_CTL 0x06000020
IMX8QM_ENET1_RGMII_TXC_CONN_ENET1_RGMII_TXC 0x06000020
IMX8QM_ENET1_RGMII_TXD0_CONN_ENET1_RGMII_TXD0 0x06000020
IMX8QM_ENET1_RGMII_TXD1_CONN_ENET1_RGMII_TXD1 0x06000020
IMX8QM_ENET1_RGMII_TXD2_CONN_ENET1_RGMII_TXD2 0x06000020
IMX8QM_ENET1_RGMII_TXD3_CONN_ENET1_RGMII_TXD3 0x06000020
IMX8QM_ENET1_RGMII_RXC_CONN_ENET1_RGMII_RXC 0x06000020
IMX8QM_ENET1_RGMII_RX_CTL_CONN_ENET1_RGMII_RX_CTL 0x06000020
IMX8QM_ENET1_RGMII_RXD0_CONN_ENET1_RGMII_RXD0 0x06000020
IMX8QM_ENET1_RGMII_RXD1_CONN_ENET1_RGMII_RXD1 0x06000020
IMX8QM_ENET1_RGMII_RXD2_CONN_ENET1_RGMII_RXD2 0x06000020
IMX8QM_ENET1_RGMII_RXD3_CONN_ENET1_RGMII_RXD3 0x06000020
>;
};
Solved! Go to Solution.
Hello,
Thank you for the community apport, this will help people with the same issue.
Best regards.
Hello,
Thank you for the community apport, this will help people with the same issue.
Best regards.