SGTL5000 datasheet formula error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000 datasheet formula error

1,018件の閲覧回数
erikfriesen
Contributor II

Page 56 of the sgtl5000 datasheet has two formulas for calculating the attack and release rate.  They both don't work for me.

Excel calcs are

#1 = (1-(10^(-(A9/(20*B9))))*2^19) and the result for (A9 or rate_dBs = 32) and (B9 or SYS_FS = 44.1) = -482267 or FFFFF8a425

#1 = (1-(10^(-(A9/(20*B9))))*2^19) and the result for (A9 or rate_dBs = 32) and (B9 or SYS_FS = 1) = -13168 or FFFFFFCC90

Raw formula says (1 - (10^(-(Rate_dBs/(20*SYS_FS)))) * 2^19

Anyway, this formula shouldn't be this complex.  Just give the clock calculations and the math should be straitforward.

タグ(1)
3 返答(返信)

800件の閲覧回数
art
NXP Employee
NXP Employee

I have checked the formula, it is correct. The point is that the SYS_FS value in the formula should be specified in the units of Hz, not kHz. So, for example, for the sampling rate of 48kHz (48000Hz) and attack rate of 32dB/s the calculation is:

(1-(10^(-(32/(20*48000)))))*524288 = approx. 40.239 = approx. 40 = 0x28

that corresponds to the example value, given in the Data Sheet document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

800件の閲覧回数
erikfriesen
Contributor II

Well, I suppose I should have tried adding the ')' where you did, but look at the datasheet again, the closing ')' is missing

800件の閲覧回数
erikfriesen
Contributor II

Just throwing out some guesses

Its an overflow ticker, so

#1 = 0x10000 / Clock * dBsecond

#2 = 0x100000 / Clock * dBsecond

These come out in the ballpark anyway.

0 件の賞賛
返信