SDRAM on IMXRT1176 EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM on IMXRT1176 EVK

ソリューションへジャンプ
611件の閲覧回数
smartpavan333
Contributor I

Hi,

I am using IMXRT1176-EVK-Board.

I am taking SDK example of sdjpeg.

In EVK board two SDRAM's but  we want to run the sdjpeg example run on single SDRAM.

0x00-SDRAM CS0.
0xFF - Full configuration. Must configure all fields.

Where should I modify? 

Note: I am Using IAR IDE.

Can you help me this issue?

0 件の賞賛
返信
1 解決策
598件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You might want to limit the SEMC size for SDRAM to only be only 256Mb so only one memory is used. This can be done on MIMXRT11##xxxxx_sdram.icf file.

Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
599件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You might want to limit the SEMC size for SDRAM to only be only 256Mb so only one memory is used. This can be done on MIMXRT11##xxxxx_sdram.icf file.

Best regards,
Omar

0 件の賞賛
返信