SDIO CMD53 is failing in i.MX6 WEC7 paltform.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDIO CMD53 is failing in i.MX6 WEC7 paltform.

1,591 次查看
qwertywifi
Contributor I

CMD53 is failing in WEC7 i.MX6 platform. I am able to read the card id of the SDIO Wi-Fi card. But last bit is coming wrong.

Please give me some suggestions.? Or is there any patch to fix this issue.?

标签 (2)
7 回复数

1,050 次查看
justin_jiang
NXP Employee
NXP Employee

Hi meton,

Where did you get the WEC7 BSP for i.MX6? Can the SD port used to read SD/MMC card?

B.R

Justin.

1,050 次查看
meflo
Contributor II

Hi Justin,

I'm trying on a 4.2.2 android, using an i.mx6 quad board.

Yes, the SD port can be used to read from a SD card.

Thanks

0 项奖励
回复

1,050 次查看
justin_jiang
NXP Employee
NXP Employee


Hi Meton,

I got confused about your issue. Is this issue only happen on WEC7 or both Android/WEC7 have this issue?

B.R

Justin

1,050 次查看
justin_jiang
NXP Employee
NXP Employee

Hi meton,

I saw you write WEC7. Which board are you using. On Freescale i.MX6 Sabre SD board we can use the SDIO WIFI card.


B.R

1,050 次查看
YixingKong
Senior Contributor IV

Qwerty

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the

issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 项奖励
回复

1,050 次查看
meflo
Contributor II

Hi Yixing,

yes we still have the issue.

0 项奖励
回复

1,050 次查看
YixingKong
Senior Contributor IV

Hi Meton

I will branch your question to internal group and assign an engineer to work on it.

Regards,

Yixing

0 项奖励
回复