refer to the bsp code, it seems
the bit24 is Standard tuning circuit and procedure enable
This field is used to enable standard tuning circuit and procedure.
bit 16-18:TUNING_STEP
The increasing delay cell steps in tuning procedure
bit 7:
Disable command check for standard tuning
Writing 1 to this field disables command check (command CRC, CMD end bit error, and CMD index error
or CMD timeout error) for standard tuning flow after each tuning command is sent
bit0-6:
Tuning start
The start delay cell point when send first CMD19 in tuning procedure
Hello,
Could you please be more specific? Where have you seen this register before, in which document of which products? I cannot find it in the reference manual of the i.MX 8X as you mentioned.
BR,
Ivan.
Hello, Ivan
Thanks for help. Also I can not find any information about the register in the reference document.
But I found the definition in the BSP source code offered by QNX.
According to the description, this register should be related with the DLL tunning for eMMC.
I think this register was not publicly documented.
Could you please check this internally?
Thank you!
yes, I couldn't find this in the RM either, but maybe you can refer to the bsp, which defines this, and use this as the bsp mentions:
#define ESDHC_TUNING_CTRL 0xcc #define ESDHC_STD_TUNING_EN (1 << 24) /* NOTE: the minimum valid tuning start tap for mx6sl is 1 */ #define ESDHC_TUNING_START_TAP_DEFAULT 0x1 #define ESDHC_TUNING_START_TAP_MASK 0x7f #define ESDHC_TUNING_CMD_CRC_CHECK_DISABLE (1 << 7) #define ESDHC_TUNING_STEP_MASK 0x00070000 #define ESDHC_TUNING_STEP_SHIFT 16
refer to the bsp code, it seems
the bit24 is Standard tuning circuit and procedure enable
This field is used to enable standard tuning circuit and procedure.
bit 16-18:TUNING_STEP
The increasing delay cell steps in tuning procedure
bit 7:
Disable command check for standard tuning
Writing 1 to this field disables command check (command CRC, CMD end bit error, and CMD index error
or CMD timeout error) for standard tuning flow after each tuning command is sent
bit0-6:
Tuning start
The start delay cell point when send first CMD19 in tuning procedure