SD3 SD3.0 slot on 6SX SABRE-SDB issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD3 SD3.0 slot on 6SX SABRE-SDB issue

877 Views
venkatesh_dyaga
Contributor II

Hi,

Board: 6SX SABRE SD

Image: Prebuilt image from i.MX 6SoloX SABRE Development Board | NXP board support packages L4.1.15_2.0.0_iMX6SX

We have been working for SDIO3 SDR104 bring up of our SDIO3.0 supported module by inserting into SD3 SD3.0 slot.

What we observed when booting is

/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode

Full log is attached which is logged on putty.

Could you please checkout and tell the error?

Thanks,

Venkatesh

Labels (1)
0 Kudos
5 Replies

727 Views
igorpadykov
NXP Employee
NXP Employee

Hi  venkatesh

from attached SDR104_not_working.zip log:  "Linux version 4.1.44-fslc"..

so seems this is not nxp official bsp, suggest to try with nxp demo images;

Linux Binary Demo Files - i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i....

Also one can try with brand new SD3.0 card, as for SDIO3.0 supported module

one can check with logic analyzer its response during initialization.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

728 Views
venkatesh_dyaga
Contributor II

Hi igorpadykov,

We will try the methods you pointed.

But I want to tell that the log I have attached is with the Yocto fsl_community_bsp build and I am sorry for that.

Now I have attached the log with NXP demo L4.1.15_2.0.0_iMX6SX image from the link I pointed in question raised.

We are trying with the SDIO3.0 SDR104 supported board.

Can you please take look at the log once and point us that whether issue exists with the kernel image?

Thanks,

Venkatesh

0 Kudos

726 Views
igorpadykov
NXP Employee
NXP Employee

Hi Venkatesh

according to Chapter 32 MMC/SD/SDIO Host Driver attached Linux

Manual MMC/SD/SDIO Host Driver does not support SDIO3.0, only

SDIO 2.0.

Best regards
igor

0 Kudos

726 Views
venkatesh_dyaga
Contributor II

Hi,

We see that there is a latest update 4.14 Yocto SUMO. Can we build that for SDR104? Can you provide any way forward to bring up our SD3.0 SDR104 board?

Thanks,

Venkatesh

0 Kudos

726 Views
igorpadykov
NXP Employee
NXP Employee

NXP L4.14.78 MMC/SD/SDIO Host Driver has the same features

for SDIO as described in Linux Manual for that release

Linux L4.14.78_1.0.0 Documentation

Best regards
igor

0 Kudos