Hi,
I have a iwave device which is based on i.mx6ul having nand.
Machine model: iW-RainboW-G26P Board based on Freescale i.MX6UL
How do I make a yocto build for this? Which document and codebase to follow?
What should be the compatible 'MACHINE' variable in local.conf?
Thanks,
Pronoy
Hello Pronoy,
This board is supported by iWave. You can see it’s webpage on the link below:
https://www.iwavesystems.com/obd-ii-connected-car-device.html
Their brochure indicates Linux 3.14.38. I would expect their BSP to be based on Yocto, in which case you should be able to use the machine configuration of it as a starting point. They should be able to provide more inputs on this.
https://www.iwavesystems.com/downloads/company-brochure/iWave-Consolidated-Brochure-R3.0.pdf
Regards,