hi all,
I am trying to use sd2 card slot for my wifi module (BCM43241 from broadcom)
but I could not be able to read or write to the module
at the boot time it is giving the following logs
mmc_attach_sdio():
wifi_set_power = 1
mmc_attach_sdio():
wifi_set_carddetect = 1
ehci_fsl_bus_suspend begins, Host 1
ehci_fsl_bus_suspend ends, Host 1
F1 signature read @0x18000000=0xffffffff
dhdsdio_probe_attach: si_attach failed!
dhdsdio_probe: dhdsdio_probe_attach failed
I tried to insert SD card and test even for the SD card also it is giving the following error
mmcblk1: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
I tried changing the SDIO data to
static const struct esdhc_platform_data mx6q_sabresd_sd2_data __initconst = {
//.cd_gpio = SABRESD_SD2_CD,
//.wp_gpio = SABRESD_SD2_WP,
.always_present = 1,
.keep_power_at_suspend = 1,
.support_8bit = 0,
.delay_line = 0,
.cd_type = ESDHC_CD_PERMANENT,
//.runtime_pm = 1,
};
but no use
Did anybody tried integrating BROADCOM or any other WIFI module on SD2 slot
If tried Kindly share me if I need to change anything
In schematics for sabereSD
I am finding in pgno 15 as
The developer
may need to consult the datasheet
of other WIFI solutions for compatibility
with this card socket.
is it mean the socket will support only few cards if that is the case kindly let me know whether BCM43241 will support on this socket or not
Regards
Reddy
Original Attachment has been moved to: logs_wifi_card_mmc_sd2.txt.zip
解決済! 解決策の投稿を見る。
Hello,Reddy,
From log messages, It seems that mmc1 didn't find new attached device(wifi) at the beginning, So could you try to power up wifi in BSP file ? At first, we should ensure mmc controller can find wifi .
weidong
Hello,reddy,
Please try to compile wifi driver into a single module, such as dhd.ko file. then use insmod dhd.ko "here is firmaware", for example, I load BCM4329 on command line:
# /system/bin/insmod /system/lib/modules/dhd.ko "firmware_path=/system/etc/wifi/sdio-bcm4329-dhd.bin nvram_path=/system/etc/wifi/nvram.txt"
Regards,
Weidong
Hi,Reddy,
Did you resolve wifi issue ?
weidong
Hi weidong sun,
There are some problems with building as a module I am working on that.
Mean while Kindly let me know how it is different from loading as a static.
Do you mean SDIO core is going to load after bcmdhd?
Kindly note: I am able to detect the card on SD3 slot by following same procedure ( loading as a static), the problem is only with the SD2, even on SD2 it is detecting the card and it is reading wrong signature F1 signature read @0x18000000=0xffffffff
and another thing is SD card is not working by giving -110 error
mmcblk1: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
soon I will update on building as loadable module scenario
Thanks
Reddy
Hi
If I am loading as a module I am getting the following error
insmod: init_module 'bcmdhd.ko' failed (No such device)
and the driver is not loading i.e it is not showing in lamod
and for the SD card the error is same -110
log is at
Regards
Reddy
Hello,Reddy,
From log messages, It seems that mmc1 didn't find new attached device(wifi) at the beginning, So could you try to power up wifi in BSP file ? At first, we should ensure mmc controller can find wifi .
weidong
Hello,Reddy,
How about your questions ? Did you resolve it ?
weidong
Hi weidong,
The problem is resolved now As you said the mmc not finding wifi device
yes there is some problem with reset pin once that is resolved it is solved
Thanks for the help
Regards
Reddy
Hello,
I am also facing the similar issue.
Could you please tell me what was the issue with the reset line?
What is the changes you have done to resolved the issue.
Regards,
Anil