SD1_DATA mux mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD1_DATA mux mode

817 Views
endl
Contributor II

Hello

I'm trying to use the "iMX 6Series Plarform SDK v1.1.0" for my demo board with iMX6DL processor.

There is a function  void hdmi_tx_phydtb_pgm_iomux(void)  from the file /board/common/board_hdmi.c.

This function configures mux mode to ALT6 for SD1_DATA0 pad and SD1_DATA1 pad ( // for hdmi_tx instance OPHYDTB[0]/OPHYDTB[1] port ??? ).

I have not found this mux mode for SD1_DATA pad from Reference Manual

FieldDescription

2–0

MUX_MODE

MUX Mode Select Field.

Select 1 of 3 iomux modes to be used for pad: SD1_DAT0.

000 ALT0 — Select signal SD1_DATA0.

011 ALT3 — Select signal GPT_CAPTURE1.

101 ALT5 — Select signal GPIO1_IO16.

What makes this setting ? And what is the OPHYDTB ? Thank you

Labels (2)
0 Kudos
Reply
1 Reply

733 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

these signals are hdmi test signals, mux mode ALT6 was removed from latest RM,

described in sect.35.7.31 Digital Transmission Mode (HDMI_PHY_DIGTXMODE) IMX6SDLRM

hdmi.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------