Dear Sir or Madam,
Hello.
My customer wants to keep only VDD voltage for SD card during 256 ms, to prevent data destruction at the power off.
(i.e. NVCC_SD is Low. VDD voltage was kept for 256 ms)
But, because DATA3 of SD card has internal pull-up, the leak voltage occurs via SD_DATA3 and NVCC_SD line.
There are possibility that the leak voltage occurs about SD_DATA3=700[mV] and NVCC_SD=150[mV] during power off to 256ms by customer's measured data on the their past i.MX6 product.
*Refer to attache file.
[Question]
If the system drops on 0[V] by next time power on, is there possibility of the latch-up of i.MX6?
Best Regards,
Keita
已解决! 转到解答。
The i.MX6 Series Hardware Development Guide document states that no I/O signals of the processor should be driven by any external voltage when the corresponding NVCC_xxx supply is powered off. So, the solution, implemented by your customer, is not allowed. The better way seems to properly shut down a SD card in software before powering off the whole system.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The i.MX6 Series Hardware Development Guide document states that no I/O signals of the processor should be driven by any external voltage when the corresponding NVCC_xxx supply is powered off. So, the solution, implemented by your customer, is not allowed. The better way seems to properly shut down a SD card in software before powering off the whole system.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------