Hi All,
I am facing following crash while trying to boot kernel uImage:
U-Boot 2014.04-08643-gbec78ae-dirty (Mar 23 2015 - 18:32:51)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 35 C, calibration data: 0x5c75227d
Reset cause: POR
Board: MX6-Sabreauto revA
I2C: ready
DRAM: 2 GiB
NAND: 0 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=12
mmc1 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
5587480 bytes read in 686 ms (7.8 MiB/s)
49698 bytes read in 47 ms (1 MiB/s)
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.72+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5587416 Bytes = 5.3 MiB
Load Address: 12000000
Entry Point: 12000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
XIP Kernel Image ... OK
Using Device Tree in place at 18000000, end 1800f221
arun changes
arunk hard-coding ldo_bypass
switch to ldo_bypass mode!
Starting kernel ...
undefined instruction
pc : [<12000008>] lr : [<8ff473a8>]
sp : 8f542b10 ip : 0000000c fp : 00000000
r10: 8f85cbac r9 : 8f542efc r8 : 00000000
r7 : 00000000 r6 : 12000000 r5 : 8ffa7da8 r4 : 00000000
r3 : 0000c222 r2 : 18000000 r1 : 00000dc9 r0 : 8f542fac
Flags: nZCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...
resetting ...
U-boot branch: imx_v2014.04_3.10.53_1.1.0_ga
Kernel: 3.10.72 (3.19.53_1.1.0_ga + Stable Updates)
I am successfully able to boot the zImage. The problem is only when trying to boot uImage.
Everything works fine when I use u-boot from branch imx_2014.04_3.10.31_1.1.0_beta branch. I have tried to root-cause the issue, I have tracked down to one-commit "404fd02 ENGR00326277-1: imx6: ldo_bypass: fix VDDARM voltage setting violate datasheet", which might be causing the issue. Can you please help further debugging and root-causing the issue.