Hello Friends,
I am trying to build u-boot on sabre sd platform through sd card(8 GB) and had downloaded the source code from git clone git://git.denx.de/u-boot.git . Compilation of the source code is successful and also uboot.imx created.Then, i tried to copy the uboot.imx using below command:
sudo dd if=u-boot.imx of=/dev/sdb bs=1k seek=1;
sync
After that i tried booting on the board from card , nothing is coming on the serial console.
Please , provide me guidelines.
Regards & Thanks
Kapil Kumar
HI Kapil
one can try uboot from official release (uboot-imx-imx_v2014.04):
Board Support Packages (27)
L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)
then follow guidelines from Linux Guide, included in that package
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------