Hi,
As mentioned in IMX6SLRM , Table 8-11. :
"eMMC reset enabled via SD_RST pad (on USDHC3 and USDHC4 only)"
1. So does it mean, if eMMC is mounted in SoloLite EVK then whenever Por_b is asserted then the eMMC will not reset since SD2 is used ?
2. eMMC reset won't be availble if using USDHC1 and USDHC2 ?
Please clarify. Thanks.
--Pankaj Rana
Hi Pankaj
1. Por_b does not affect SD_RST. eMMC will be reset by Power Cycle
or SD_RST (H/W RESET) according to emmc specifications.
2. if using USDHC1 and USDHC2 only Power Cycle reset is available.
In general one can use any gpio for usage as SD_RST.
Details about SD_RST can be found on link below
About SDa_RST_B (SD3_RST) signal in i.MX6.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------