SABRE i.MX7 Bluetooth Chipset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE i.MX7 Bluetooth Chipset

1,207 Views
christopheferra
Contributor I

Hi,

I wonder what BT and wifi chipset are on the SABRE i.MX7 development board. My board is 700-28590 REV D.

I want to use Bluez and the BLE chipset should be supported.

Best regards,

Christophe

0 Kudos
Reply
4 Replies

1,108 Views
christopheferra
Contributor I

Linux

If i know the chipset model, i can afford with this.

0 Kudos
Reply

1,108 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the 4.14.78 linux release note:

Supports Murata Cypress Wi-Fi/Bluetooth (BCM4339) on i.MX 6 and i.MX 7Dual.

L4.14.78_1.0.0_LINUX_DOCS ” from the “Supporting Information

0 Kudos
Reply

1,108 Views
christopheferra
Contributor I

Thanks

0 Kudos
Reply

1,108 Views
joanxie
NXP TechSupport
NXP TechSupport

what OS do you need? linux or android?

0 Kudos
Reply