SABRE AI edige connector

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE AI edige connector

2,158件の閲覧回数
tmatsuzawa
Contributor I

Is anyone aware of easy solution to break out signals available on ESABRE AI board's edge connector (281 pins) so that I can try something.

The below post says there is a debug line breakout board for this.

I want to do similar, but with different line signals.

https://community.freescale.com/message/392960

The schematics says the socker prt # is follows, but it seems it is not easy to get at DYI shops.

SPEEDTECH CORP

B35P101-01123-H

It's 0.5mm pitch, and maybe it could not be exactly be this part #, but currently have no idea of what easy-to-get connector kit is compatible with it.

Or, freescale has something (part kit) that can be used?

I know SABRE AI base board has socket for it, but I try to use SABRE AI CPU board standalone.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,906件の閲覧回数
tmatsuzawa
Contributor I

Well, after some research, I believe it is MXM 3.0 specification, and Wandboard's EDMCONNECTORKIT could be one option.

Any other experiences?

0 件の賞賛
返信

1,906件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Takashi Matsuzawa,

There is a thread (link below) in which they mention how they used a Speedtech B35P101-01123-H connector so that would be the safest bet. Although I understand that this part number may not be easily available.

Evalboard with i.mx6 and ETM/PTM connector

The Speedtech has a MXM 3.0 form-factor which should be the same as the EDM, which is the used on the Wandboard.

0 件の賞賛
返信