S/W encoding H.264 with i.MX7D

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S/W encoding H.264 with i.MX7D

跳至解决方案
1,228 次查看
ScottKerstein
Contributor III

Hello,

Looking to encode H.264 from a 1080p30fps imager on the i.MX7D using GStreamer.  Is there a way to determine the CPU utilization and if a Cortex-A7 running at 1.2GHz is enough to do this task?  This is the only task.  

Thanks, in advance.

Scott

标签 (4)
0 项奖励
回复
1 解答
1,080 次查看
ScottKerstein
Contributor III

Thanks, Igor.  Looks like it will be limited to just JPEG in software.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,080 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Scott

nxp linux video performance without vpu is described in attached Release Notes

Table 31. Video codec specification for hardware without VPU acceleration.

More details about VPU versus non-VPU analysis  can be obtained creating service request

Support|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,081 次查看
ScottKerstein
Contributor III

Thanks, Igor.  Looks like it will be limited to just JPEG in software.

0 项奖励
回复