Hello All,
I am trying to run the camera test and wants a yuv file.
I have flashed the images on imx6ull evk board with ov5640 sensor and boot the board.
After that i ran the capture test with below command.
/unit_tests/mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -f 422P -i 1 ./test.yuv
It fails to run and give the following message on hyper terminal.
n_width = 640, in_height = 480
out_width = 640, out_height = 480
top = 0, left = 0
VIDIOC_DBG_G_CHIP_IDENT failed.
get format failed
I did insmod these files:
adv7180_tvin.ko
ipu_fg_overlay_sdc.ko
mxc_mipi_csi.ko
ov5640_camera_int.ko
ov5647_camera_mipi.ko
fbdev ipu_prp_enc.ko
mxc_v4l2_capture.ko
ov5640_camera_mipi.ko
v4l2-int-device.ko
ipu_bg_overlay_sdc.ko
ipu_still.ko mxc_vadc.ko
ov5640_camera_mipi_int.ko
ipu_csi_enc.ko
mx6s_capture.ko
ov5640_camera.ko
ov5642_camera.ko
but also had err;
what can i do?
can any one guide me why it fails to capture using camera? is there anything missing?
pls refer to the link as below: