Hi Guys,
I need to run camera app as background java service in Android9, IMX8qxp. For which I use built-in camera app as background service and trying to run in background at BOOT_COMPLETE.
I am facing this crash, few times on reboot
============================================================================
--------- beginning of crash
04-13 15:16:31.790 3131 3221 F libc : Fatal signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0xe0000c in tid 3221 (MessageThread), pid 3131 (provider@2.4-se)
04-13 15:16:31.740 3131 3221 I chatty : uid=1047(cameraserver) MessageThread identical 1 line
04-13 15:16:31.782 3131 3221 I FslCameraHAL: handleFrameByOpencl:688, opencl don't support format convert from 0x25 to 0x103
04-13 15:16:31.893 4062 4062 I crash_dump32: obtaining output fd from tombstoned, type: kDebuggerdTombstone
04-13 15:16:31.895 3178 3178 I /system/bin/tombstoned: received crash request for pid 3221
04-13 15:16:31.901 4062 4062 I crash_dump32: performing dump of process 3131 (target tid = 3221)
04-13 15:16:31.914 4062 4062 F DEBUG : *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
04-13 15:16:31.915 4062 4062 F DEBUG : Build fingerprint: 'Android/mek_8q/mek_8q:9/2.3.0-ga-rc2/wasim.nazir04131243:userdebug/dev-keys'
04-13 15:16:31.915 4062 4062 F DEBUG : Revision: '0'
04-13 15:16:31.915 4062 4062 F DEBUG : ABI: 'arm'
04-13 15:16:31.915 4062 4062 F DEBUG : pid: 3131, tid: 3221, name: MessageThread >>> /vendor/bin/hw/android.hardware.camera.provider@2.4-service <<<
04-13 15:16:31.915 4062 4062 F DEBUG : signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0xe0000c
04-13 15:16:31.916 4062 4062 F DEBUG : r0 00e0000c r1 00e00000 r2 e9a80000 r3 e9ad0e00
04-13 15:16:31.916 4062 4062 F DEBUG : r4 e9a80000 r5 00e00000 r6 eb813308 r7 e9ad0e00
04-13 15:16:31.916 4062 4062 F DEBUG : r8 00e0000c r9 e9ad0e00 r10 ea5db448 r11 00000000
04-13 15:16:31.916 4062 4062 F DEBUG : ip ec16e62c sp ea5db390 lr ec133ea5 pc ec12e540
04-13 15:16:31.942 4062 4062 F DEBUG :
04-13 15:16:31.942 4062 4062 F DEBUG : backtrace:
04-13 15:16:31.943 4062 4062 F DEBUG : #00 pc 00064540 /system/lib/libc.so (pthread_mutex_lock+4)
04-13 15:16:31.943 4062 4062 F DEBUG : #01 pc 00069ea1 /system/lib/libc.so (je_arena_dalloc_large+20)
04-13 15:16:31.943 4062 4062 F DEBUG : #02 pc 0007df39 /system/lib/libc.so (je_free+72)
04-13 15:16:31.943 4062 4062 F DEBUG : #03 pc 0001755f /system/lib/vndk-sp-28/libhwbinder.so (android::hardware::Parcel::freeDataNoInit()+182)
04-13 15:16:31.943 4062 4062 F DEBUG : #04 pc 00017491 /system/lib/vndk-sp-28/libhwbinder.so (android::hardware::Parcel::~Parcel()+4)
04-13 15:16:31.943 4062 4062 F DEBUG : #05 pc 00010931 /system/lib/vndk-28/android.hardware.camera.device@3.4.so (android::hardware::camera::device::V3_4::BpHwCameraDeviceCallback::_hidl_processCaptureResult_3_4(android::hardware::IInterface*, android::hardware::details::HidlInstrumentor*, android::hardware::hidl_vec<android::hardware::camera::device::V3_4::CaptureResult> const&)+364)
04-13 15:16:31.943 4062 4062 F DEBUG : #06 pc 00010b33 /system/lib/vndk-28/android.hardware.camera.device@3.4.so (android::hardware::camera::device::V3_4::BpHwCameraDeviceCallback::processCaptureResult_3_4(android::hardware::hidl_vec<android::hardware::camera::device::V3_4::CaptureResult> const&)+14)
04-13 15:16:31.943 4062 4062 F DEBUG : #07 pc 00010a03 /vendor/lib/camera.device@3.4-impl.so (android::hardware::camera::device::V3_4::implementation::CameraDeviceSession::ResultBatcher_3_4::invokeProcessCaptureResultCallback_3_4(android::hardware::hidl_vec<android::hardware::camera::device::V3_4::CaptureResult>&, bool)+410)
04-13 15:16:31.943 4062 4062 F DEBUG : #08 pc 00010495 /vendor/lib/camera.device@3.4-impl.so (android::hardware::camera::device::V3_4::implementation::CameraDeviceSession::ResultBatcher_3_4::processOneCaptureResult_3_4(android::hardware::camera::device::V3_4::CaptureResult&)+172)
04-13 15:16:31.943 4062 4062 F DEBUG : #09 pc 0000fe53 /vendor/lib/camera.device@3.4-impl.so (android::hardware::camera::device::V3_4::implementation::CameraDeviceSession::ResultBatcher_3_4::processCaptureResult_3_4(android::hardware::camera::device::V3_4::CaptureResult&)+106)
04-13 15:16:31.943 4062 4062 F DEBUG : #10 pc 0000d8f7 /vendor/lib/camera.device@3.4-impl.so (android::hardware::camera::device::V3_4::implementation::CameraDeviceSession::sProcessCaptureResult_3_4(camera3_callback_ops const*, camera3_capture_result const*)+746)
04-13 15:16:31.943 4062 4062 F DEBUG : #11 pc 00009a9b /vendor/lib/hw/camera.imx8.so (CaptureRequest::onCaptureDone(StreamBuffer*)+90)
04-13 15:16:31.943 4062 4062 F DEBUG : #12 pc 0000b37f /vendor/lib/hw/camera.imx8.so (VideoStream::processCaptureRequest(StreamBuffer&, android::sp<CaptureRequest>)+94)
04-13 15:16:31.943 4062 4062 F DEBUG : #13 pc 0000b101 /vendor/lib/hw/camera.imx8.so (VideoStream::handleCaptureFrame()+412)
04-13 15:16:31.943 4062 4062 F DEBUG : #14 pc 0000b50b /vendor/lib/hw/camera.imx8.so (VideoStream::handleMessage()+338)
04-13 15:16:31.943 4062 4062 F DEBUG : #15 pc 0000b655 /vendor/lib/hw/camera.imx8.so (VideoStream::MessageThread::threadLoop()+8)
04-13 15:16:31.943 4062 4062 F DEBUG : #16 pc 0000c0cb /system/lib/vndk-sp-28/libutils.so (android::Thread::_threadLoop(void*)+286)
04-13 15:16:31.943 4062 4062 F DEBUG : #17 pc 00063c15 /system/lib/libc.so (__pthread_start(void*)+22)
04-13 15:16:31.943 4062 4062 F DEBUG : #18 pc 0001e085 /system/lib/libc.so (__start_thread+22)
============================================================================
What can be the issue for the crash. Is it because the camera/media native services are not ready at BOOT_COMPLETE. Full log is attached below.
Any suggestions will be helpful.
Thanks in Advance,
Wasim
Hello wasim,
This is not supported by android BSP, however We have observed similar issue when camera was connected to the board while kernel was booting. Please try connecting USB camera after Android has booted successfully. for the backround for the apps
service - How to record video from background of application : Android - Stack Overflow
Regards